Hardware Tab - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Hardware tab shows hardware-related attributes associated with the hardware source of an integration, device, or a point (for example, when an object has a reference to a physical input or output).

Note: Each Hardware attribute table is organized and divided into sections of Integration Hardware attributes, Device Hardware attributes, and Point Hardware attributes (calling out when attributes are shared between these object types). These sections are indicated by headings that span across the table.