Focus Tab - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Focus tab appears when you define an object in the online Site Management Portal. The Focus tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Focus tab varies by object type. For example, the Analog Input object’s Focus tab has different attributes than the ODS object’s Focus tab. See the specific object section for details on its Focus tab.

Note: This tab is called the Configuration tab in the SCT or in a wizard.