Engineering Tab - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

The Engineering tab appears on integration objects in the system. This tab allows you to view and edit attributes of items such as devices and points on an integration.

To use the Engineering tab to view and edit attributes:

Procedure

  1. Right-click the integration object on the Navigation tree and select View. The Integration object appears.
  2. Click the Engineering tab, and navigate to an item in the Integration Tree.
    Note: You may need to click Relearn to discover the integrated devices and points on the network and populate the Integration Tree with the data.
  3. Double-click the selected item. The Details screen for the selected item appears.
  4. Click the Edit button.
  5. Make the desired changes and click Save.