Configuration Tab - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Configuration tab appears when you define an object in the SCT or in a wizard. The Configuration tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Configuration tab vary by object type. For example, the Analog Input object’s Configuration tab has different attributes than the ODS object’s Configuration tab. See the specific object section for details on its Configuration tab.

Note: This tab is called the Focus tab in the online Site Management Portal.