Object and Feature Tabs - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

This section describes the tabs of the display panel for the objects and features in the system. Each display panel can contain different tabs depending on the item being viewed, and each tab shows different information.

Note: This section contains detailed information about the tabs used by multiple objects/features. When a tab only appears for a specific object/feature, the details of that tab are defined in that object/feature section. However, this section includes a brief description of such tabs and provides links to the detailed object/feature sections.