State, Mode, and Type Sets - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

State, Mode, and Type Sets provide the source of readable text for the user interface when the displayed value can be one of many states, modes, or types. For example, the Status attribute of every object is displayed as one of the texts listed in the Object Status (Set 505).

References to specific sets appear throughout the Object Help, usually in the Values/Options/Range column of the object’s attribute table.