Object Naming Attributes - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Every object can be identified by one of three naming attributes.

Name - a freely definable user name for the object

Item Reference - a fixed name used internally by the system

BACnet Object Name - the name exposed to a BACnet network based on the Item Reference, or the name based on the User Name Is BACnet Obj Name common attribute setting

See the Object and Feature Tabs section for more information on these attributes.