Object Extensions - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Object extensions provide additional features to objects and include Alarm, Trend Log, Totalization (Analog, Runtime, and Event), Load, Averaging, and Resource File. Object extensions do not appear in the navigation tree. The attributes of Object Extensions are displayed under specific tabs when viewing object details. You may define object extensions when the object is first created using the configuration wizard or add them later.

For more information on extensions, see the Extensions section.