Object Deletion - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Objects can be deleted offline in the system database on the SCT and later downloaded to the host device as part of the edited database. You can also delete objects with a browser if you have the Access Privileges to configure objects using the Security Administrator System. The user interface screens and procedures are similar in either case. Deleting an object involves selecting it in the Navigation Tree and using the Delete Items command.

See the Deleting Objects or Items section for more information.

Note: Before deleting an object, you should delete all references to the object within other objects and reconfigure any objects that are referenced in the object to be deleted. If the references are not edited or deleted, the referenced objects may not operate correctly. See the Engine Device Object for an example of how to locate incomplete references.