Object Creation - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Objects can be created offline in the system database on the SCT and later downloaded to the host device as part of the edited database. You can also create objects with a browser if you have the Access Privileges to configure objects using the Security Administrator System. The user interface screens and procedures are similar in either case. Creating an object involves placing it at the desired position in the Navigation Tree and defining all the attributes that are required for it to operate. The procedure begins with the Insert Menu, and a wizard guides you through all the necessary configuration steps.

See the Creating Items with Wizards section for the steps to create objects/items.