Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Commands table for each object lists the commands that the object supports. Commands allow you to perform an action on an object, such as Start or Stop. The user executes these commands through the user interface. If an object does not support any commands, the Commands table does not appear in the Help. For a description of each command, click the command name in the Commands table.

The column headings in the Commands table are defined as follows:

Command Name - Gives the name of the command as it appears in the user interface.

Parameters - Gives the parameters required in the command along with some descriptive information.