Values/Options/Range - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Based on the attribute’s data type, this column may show the range of valid values or a reference to the set of possible values for this attribute. If the complete set of values for the attribute is small, all possible values are shown in this column.