The BACnet Notes column specifies if the attribute is exposed as a standard BACnet property and if it can be modified from a BACnet network.
|
Note |
Definition |
|---|---|
|
B - Exposed as Standard BACnet Property |
Indicates that the attribute can be accessed as a standard BACnet Property of the equivalent BACnet Object Type from a BACnet network. |
|
W - Writable |
Indicates that the value of the attribute can be modified by a message from a device on the BACnet network. |
Note: The types listed in Table 1 may also appear in the Note column,
as applicable.