Multiple Command Commands - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The table below lists the commands supported by this object.

Table 1. Multiple Command Object Commands

Command Name

Parameters

Dscription

Disable

None

Specifies that (when the Multiple Command object is disabled) outputs are locked and commands are prevented from being sent.

Enable

None

Specifies that (when the Multiple Command object is enabled) the object it is capable of issuing commands.

Multistate0...Multistate31

None

Releases Command Priorities 9 through 15 (Scheduling) and then writes to the Present Value at the Default (16) command priority. The state command names and number of commands are dependent on the States Text and Number of States attributes.

Operator Override

State 0–31

Updates the Present Value at Command Priority Operator Override.

The Operator Override command sends the specified command to the internal NxE object, which is then only sent to the field device when one of the following conditions is met: a) NOT Local Control and NOT Out Of Service, or b) NOT Local Control and after issuing the In Service command.

Release

  1. Attribute name
  2. Command priority

Releases the identified command priority from the specified, writable attribute, and allows it to be controlled by the next highest priority.

Release All

Attribute name

Releases Command Priorities 3 through 16 from the specified, writable attribute. Command Priorities 1 (Manual Emergency) and 2 (Fire Application) remain.

Important: The Release All command may not cause an immediate return to automatic operation. The Release All command clears all command priorities, including those that come from applications and features. When this happens, the output point goes to its Relinquish Default condition. In some cases, the application or feature may have sent a command that does not match Relinquish Default. In this instance, the output point does not end in the state that the applications or features intended. This situation can cause unexpected operation to occur; for example, a space could overcool or overheat, a fan might run longer than expected, and so on. If an operator has overridden an input, use the Release Operator Override command.

Release Operator Override

None

Releases Command Priority Operator Override from Present Value.