Interlock Configuration - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Configure the attributes of the Focus/Configuration, Interlock Definition, and Action Tables tabs of the Interlock object. See the Interlock Attributes section for descriptions of the attributes on these tabs.

On the Focus/Configuration tab, click the Advanced radio button to view and edit all the attributes available on this tab.

On the Interlock Definition tab, define the items/objects to control and the desired conditional logic.

Tips for this tab include:

  • Click the Add button to add items to the list from the Select Item dialog box. You can also select items from the All Items tree or from the Global Search results and drop them into the Interlock Definition table.

  • Click the check box next to an item in the list and click Delete to remove the item from the list.

  • Select the type of logic to use for the items in the list from the Logic menu. See the Logic attribute description for the types of logic.

On the Action Tables tab, define the commands and the priority for the items/objects under control.
Figure 1. Example of Interlock Action Table Headers and Options

Tips for this tab include:

  • Check the All Commands Priority check box if you wish to use the same priority for all commands in the action tables. Clear the All Commands Priority check box to enable individual priority selection for the commands in the action tables.

  • Check the Add New Items to All Conditions check box if you wish to add new items to both the Actions for Condition: True and Actions for Condition: False tables. The Add New Items to All Conditions is selected by default.
  • For the Actions for Condition: True and Actions for Condition: False tables, click the Add button to add items to the table from the Select Item dialog box. You can also select items from the All Items tree or from the Global Search results and drop them into the Interlock Action tables.

  • For the Actions for Condition: True and the Actions for Condition: False tables, click the check box next to an item in the table and click Delete if you want to remove the item from the table.

  • To select all items within a table, click the Select All column header. To unselect all items within a table, click the Select All column header again.
  • To mass command items in the Actions for Condition: True or the Actions for Condition: False, select similar items that have the same configured attributes and enumerations (for example, select multiple BVs). Right-click the Command column header and click Set Command. Or, click Set Command. The Set Command for Selected Items appears.
    Figure 2. Right-Click Set Command Option

  • To mass set delay, select multiple items (can be dissimilar items), input a delay in the Set Delay field, and click Set Delay.