The table below lists the commands supported by the Interlock.
|
Command Name |
Parameters |
Description |
|---|---|---|
|
Disable |
None |
Locks out all outputs and prevents the Interlock functionality. |
|
Enable |
None |
Ensures object reacts to any changes it may have missed while it was disabled, and returns it to normal operation. |
|
Operator Override |
The value to be written to the Present Value attribute. This parameter has a True or False data type. |
Updates the Present Value at Command Priority Operator Override.
Important: The Operator Override command sends the specified command to the internal NxE object, which is then only sent to the field device when one of the following conditions is met: a) NOT Local Control and NOT Out Of Service, or b) NOT Local Control and after issuing the In Service command.
|
|
Release Operator Override |
None |
Releases Command Priority Operator Override from Present Value. |
|
Re-command |
None |
Reissues the commands for the current state. |
|
Release |
Attribute name Command priority |
Releases the identified command priority from the specified, writable attribute, and allows it to be controlled by the next highest priority. |
|
Release All |
Attribute name |
Releases Command Priorities 3 through 16 from the specified, writable attribute. Command Priorities1 and 2 remain.
Note: The Release All command may not cause an immediate return to automatic operation. The Release All command clears all command priorities, including those that come from applications and features. When this happens, the output point goes to its Relinquish Default condition. In some cases, the application or feature may have sent a command that does not match Relinquish Default. In this instance, the output point does not end in the state that the applications or features intended. This situation can cause unexpected operation to occur; for example, a space could overcool or overheat, a fan might run longer than expected, and so on. If an operator has overridden an input, use the Release Operator Override command.
|