Global Data Sharing Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Global Data Sharing Object.

Table 1. Global Data Sharing Object Commands

Command Name

Parameters

Description

Disable

None

Prevents the object from responding to any change in the Master, including reliability changes.

Enable

None

Updates the Subordinates List with COVs. Immediately after receiving this command, the Master referenced value is routed to each of the output references.