Status - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Status displays an icon to indicate the current status of the load. Table 1 provides icon descriptions.

Table 1. Load Summary Icons and Their Status

Status Icon 1

Load Status



Load appears to be offline; system is awaiting confirmation.



Load is offline.



Load is disabled.



Load is shed.



Load is locked.



Load is in comfort override.

<no icon>

Load is released.

1 Positioning the mouse on an icon in the Status column displays a tooltip.