Point Name and Point Reference - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Point Name and Point Reference fields display in colors that indicate the load output’s current condition. Table 1 describes the default colors.

Table 1. Default Coloration of Point Name and Point Reference Fields

Condition of Output

Point Name and Point Reference Field Color

Normal

White

Overridden

Orange

Offline

Black

Trouble/Warning

Yellow

Alarm

Red

1 The actual colors used are set in the Status Colors section of Metasys Preferences > Graphic Settings. For details, refer to the ODS Commissioning Guide (LIT-12011944) or NAE Commissioning Guide (LIT-1201519).