Maximum Shed Time - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Maximum Shed Time (optional) specifies the maximum number of minutes that a load can be shed before it is automatically released. If the Maximum Shed Time value is not defined, the default value of 65,535 is used. The range is 0 to 65,535 minutes.