The Enabled attribute provides a mechanism to stop DLLR operation. When disabled, DLLR releases all shed loads except those that are locked shed. Also, DLLR does not perform any calculations, report alarms, or issue any commands to any loads when disabled. DLLR attributes can be changed, but no actions are taken until DLLR is enabled.
When enabled, DLLR operation starts again. If Shed mode is active, the configured DLLR strategies begin shedding loads as needed. If Monitor Only mode is configured, simulated load shedding begins.