DLLR Status - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The DLLR Status attribute indicates the current DLLR status. The statuses include:

  • Normal - no errors or problems in the DLLR object

  • LR cannot meet target - the Load Rolling algorithm was unable to shed enough loads to meet its target.

  • DL cannot meet target - the Demand Limiting algorithm was unable to shed enough loads to meet its target.

  • Meter Off Normal - a meter is defined, but it is offline or its value is not reliable.

  • EOI Off Normal - an EOI attribute is defined, but it is offline or its value is not reliable. This also indicates that the EOI Attribute is replaced with the fixed window algorithm.

  • Disabled - the DLLR object is not being used to shed (or simulate the shedding of) loads.

  • No meter defined for DL - a meter is not currently defined for DL; a requirement if the Shed Strategy includes Demand Limiting.