Smoothed ABS Error - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The smoothed absolute error is based on the forecast error and is used to provide a safety margin to prevent the interval demand from exceeding the target. It equals the average percentage of variation in the uncontrolled energy rate.