Error Limit - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Error Limit attribute limits the Smoothed ABS Error to a percentage of the Active Demand Limit. It can be used to reduce the size of the safety margin to avoid unnecessary overshedding. This value should be changed with care, since it increases the possibility of exceeding the demand limit target. The default value is 10%.