The Stop DLLR Audits in Monitor Only Mode attribute specifies whether an audit entry is created each time a load is shed or released when DLLR is in Monitor Only mode and the NAE’s Enabled Audit Level is set to 3 or 4. (When DLLR is in Active mode, an audit entry is always created to record that event.) The default is False, but if you set it to True, no audit entries are created in Monitor Only mode.