Monitor Mode Release - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Monitor Mode Release attribute allows you to specify the load output release behavior when DLLR is commanded to Monitor Only mode from Shed mode. If set to Release immediately, the outputs of loads that are not locked are immediately released regardless of whether their Minimum Shed Time has expired. If set to Release After Min Shed Time, the outputs of loads that are not locked are released only after their Minimum Shed Time expires. Possible behaviors include:

  • Release Immediately

  • Release After Min Shed Time