Mode - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Mode attribute controls whether DLLR is actively shedding Loads (Shed mode) or is simulating Load shedding (Monitor Only mode). The mode pertains to both the Demand Limiting and Load Rolling strategies simultaneously. The Modes include:

  • Monitor Only - simulated shedding occurs, where loads appear shed but output points are not actually commanded or turned off.

  • Shed - true shedding occurs where output points are commanded.