Meter Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Meter Object identifies the Metasys object (for example, Pulse Meter, AI, AV) that is used for the energy rate if the Demand Limiting strategy is configured. If only the Load Rolling strategy is used, a meter is not required.

The Meter Object should be defined on the same supervisory controller as the DLLR Object. Do not use an N1 Integration object for the meter unless you can guarantee that the NCM Service Time is always less than 60 seconds because the DLLR algorithm requires an updated meter value every minute.