LR Tariff Targets - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The LR Tariff Targets attribute lists the energy targets for the Load Rolling strategy. Each target consists of a target value and an entry from the Target Description set identifying the type of target, such as On-Peak. If the Load Rolling strategy is used, there must be at least one target defined. Only one target is active at a time. The Active LR Target attribute specifies which LR Target is currently active. The Target Description set includes:

  • Continuous

  • Off-Peak

  • On-Peak

  • Semi-Peak

  • Shoulder

  • Summer Off-Peak

  • Summer On-Peak

  • Winter Off-Peak

  • Winter On-Peak

  • Summer Semi-Peak

  • Winter Semi-Peak

  • Summer Shoulder

  • Winter Shoulder