Current LR Target - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Current LR Target attribute represents the load rolling target that is set by the user (LR Tariff Targets indexed by Active LR Target). This target defines the amount of energy that should be shed each minute for the load rolling strategy. You can change the value of the load rolling target by writing to this attribute.