Active Elevation - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Active Elevation attribute indicates the amount (in percent) by which the demand limit was increased during the elapsing interval to obtain the starting value of the demand limit profile. The Active Elevation represents the Limit Elevation that is used for the current interval.