Rate Units - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Rate Units attribute specifies the energy units used for instantaneous energy demand attributes and referenced in the DLLR Profile and Load Summary (for example, kW). If a meter is defined, the Rate Units attribute indicates the units of the meter.