Demand Interval Length - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Demand Interval Length attribute specifies the length in minutes of an interval for the Demand Limiting strategy. This value is normally obtained from the energy utility. The DLLR Interval Lengths set specifies the possible interval lengths (15, 30, or 60).