DL Tariff Targets - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The DL Tariff Targets attribute is the list of energy targets for the Demand Limiting strategy. Each target consists of a target value and an entry from the Target Description set identifying the type of target, such as On-Peak. If the Demand Limiting strategy is used, there must be at least one target defined. Only one target is active at any time. The Active DL Target attribute specifies which target is currently active. The Target Description set includes:

  • Continuous

  • Off-Peak

  • On-Peak

  • Semi-Peak

  • Shoulder

  • Summer Off-Peak

  • Summer On-Peak

  • Winter Off-Peak

  • Winter On-Peak

  • Summer Semi-Peak

  • Winter Semi-Peak

  • Summer Shoulder

  • Winter Shoulder