Algorithm - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Algorithm attribute specifies which algorithm is used for the Demand Limiting strategy (Fixed Window or Sliding Window). In most cases, the Sliding Window Algorithm is required by North American utilities, while the Fixed Window Algorithm is used by European utilities.