Active DL Target - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Active DL Target specifies which of the defined Demand Limiting targets is currently active. When this attribute changes, the Active DL Target Changed attribute indicates True until the start of the next interval. This attribute uses the Target Description enumeration set.