Allow Reset in Shed Mode - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Allow Reset in Shed Mode attribute controls whether the Reset Initialization Parameters command can be issued while DLLR is in Shed mode. When True, the Reset Initialization Parameters command can be issued once if DLLR is in Shed mode. As soon as the command is issued, this attribute is automatically reset to False and must be manually set to True before the command can be issued again in Shed mode.