Active LR Target Changed - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Active LR Target Changed attribute displays True when the Active LR Target value is changed. It is set to False at the start of the next interval if demand limiting is configured, or at the start of the next minute if load rolling only is configured. This attribute allows the DLLR object to raise an alarm when the LR target changes.