Unreliable Meter Shed Rate - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Unreliable Meter Shed Rate attribute specifies how much load the DLLR object should keep shed if the meter goes unreliable, provided the Use Unreliable Meter Shed Rate option is selected for the Unreliable Meter Options attribute.