Active DL Target Changed - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Active DL Target Changed attribute displays True when the Active DL Target value is changed. It remains True until the start of the next interval, when it is reset to False. This attribute allows an alarm to be raised when the DL target changes.