Data Broadcast Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following table lists the commands supported by the Data Broadcast Object.

Table 1. Data Broadcast Commands

Command Name

Parameters

Description

Disable

None

Locks all outputs and prevents the object from broadcasting any messages.

Enable

None

Specifies that the Data Broadcast object broadcasts Unconfirmed COV Notification messages when the Input Reference changes.