User Views with Tailored Summaries - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Tailored Summary feature relies on the User View feature to provide a mechanism for viewing Tailored Summaries. After defining Summary Definition objects, add them to a folder in the User View through the All Items tree. Then view the Tailored Summary through the User View (that is, view the User View folder to display the Tailored Summary). See the User View Editor, Workflow, and Defining User Views with Summary Definitions topics in the Tailored Summaries section in the Metasys SCT Help (LIT-12011964) .