ODS Commands - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The table below lists the commands supported by the Table 1.

Table 1. ODS Device Object Commands

Command Name

Description

Archive

Archives the object instances to the nonvolatile memory.

Change Audit Enabled Class Level Changes the Audit Enabled Class Level attribute.

Integer (1 to 4)

Route Samples

Routes all Trend samples to the Metasys Server. Use this command before performing an engine upgrade to minimize the risk of losing any trend samples.

Rediscovery Text Strings
Resets the States Text across a supervisory device by rediscovering text strings from all mapped BACnet objects.
Note: When the Rediscover Text Strings command is sent from the Site Director device UI to another supervisory device and the UI is running on the supervisory device, you must close and restart the UI on the supervisory device in order for the text to appear correctly.