Metasys Server - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Insert > Metasys Server

Inserts a Metasys server at any supported release into the archive database with SCT, including the following servers: ADS/ADX, ADS-L-A, ADS-L-E, OAS, and ODS).

Tip:
  • The first Metasys server you add to the site becomes the Site Director. The Site Director coordinates all Web browser communication to the Metasys network. You can only have one Site Director per site. Any subsequent Metasys servers are primarily used for archiving historical data.
  • On the Configure screen, select each tab for further configuration options.