The table below lists the commands supported by the VND Integration Object.
Command Name |
Description |
---|---|
Clear Statistics |
Resets the statistics for the integrated vendor network. |
Disable |
Disables the entire vendor network integration. No requests are made to the field trunk and no data broadcasts to the network are processed. |
Enable |
Allows the integration to function normally. |
Latch Statistics |
Updates the displayed statistics with the current values. |