VND Integration Attributes - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Note: In the Notes column, attributes that are marked with a letter C are configurable and attributes marked with the letter W are writable.
Table 1. VND Integration Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Description

Enabled

C,W

True

If True, allows the use of the vendor integration. If False, prevents the use of the vendor integration.

Offline

 

True

Displays the offline or online status of connected hardware.

Table 2. VND Integration Attributes - Diagnostic Tab

Attribute Name

Notes

Initial Value

Description

Count

W

0

Displays the number of vendor device and point objects defined for the trunk. This count does not include extensions.

Errors In

W

0

Indicates the number of field communication errors (bad format, for example) received. The Clear Statistics command resets this value.

Errors Out

W

0

Indicates the number of field communication attempts that failed. The Clear Statistics command resets this value.

Function Time Exceeded

 

0

Indicates the number of functions to the Vendor DLL that took longer than 100 milliseconds to execute. The Clear Statistics command resets this value.

Message Receives

 

0

Indicates the number of messages received field devices. This value resets to zero at midnight. The Latch Statistics command updates this value.

Message Transmits

 

0

Indicates the number of messages sent to field devices. This value resets to zero at midnight. The Latch Statistics command updates this value.

Permanent Status Item Count

 

0

Displays the number of items polled as a result of COV signups.

Priority 1 Poll Time

 

0

Indicates how often the items in the Priority 1 list are polled. Units = Seconds

Reset Date

   

Contains the date stamp of the last Clear Statistics command.

Reset Time

   

Contains the time stamp of the last Clear Statistics command.

Temporary Status Item Count

 

0

Displays the number of items polled.

Transmits In

 

0

Indicates the rate of transmissions received by the integration.

Transmits Out

 

0

Indicates the rate of transmissions sent by the integration.