Multiple NIEs - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Migration can be split across multiple NIEs with the following constraints:

  • Only one N1 Migration object can exist per NIE per N1 network.

  • Multiple NIEs can reference the same N1 network.

  • Only one NCM object can exist per NCM per N1 Migration object.

  • Multiple NCM objects can reference the same NCM as long as they exist on different NIEs.

  • Only one point object can exist per NIE per N1 object.

  • Multiple point objects can reference the same N1 object as long as they exist on different NIEs.