The following table lists the commands supported by the MS/TP Field Bus Integration Object.
|
Command Name |
Parameters |
Description |
|---|---|---|
|
Analyze Field Bus |
None |
Scans the entire MS/TP field bus (addresses 0–254) and compiles a list of all devices on the bus. The Analyze Field Bus command also provides configuration information for each device that responds. The data collected helps to determine devices that may be configured incorrectly and thus affect the bus performance. Because of the high bus traffic load created by the scan, this command should not be used on a regular basis. This command is primarily intended for use during commissioning. Track the progress of this analysis in the Bus Analysis Progress attribute. The results of this command appear in the Bus Device Configuration List attribute. The date and time of the last completed scan appear in the Bus Analysis Date attribute and Bus Analysis Time attribute, respectively. See MS/TP Field Bus Integration Attributes for more information about these attributes. |
|
Clear Statistics |
None |
Clears the statistics for the integrated MS/TP network. |
|
Latch Statistics |
None |
Updates the displayed statistics with the current values. |
|
Sync Field Device Time(s) |
None |
Sends a high-priority time synchronization command to all child BACnet Integration devices, based on each device mapper object's Manual Time Sync Type attribute. If the Manual Time Sync Type is set to:
|