This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).
|
Attribute Name |
Data Type |
Description |
|---|---|---|
|
Bind Retry Count |
Number |
Indicates the number of objects for which the Lon Integration code is still verifying with the field controller that it has the correct type information. |
|
Count |
Number |
Displays the number of LonWorksnetwork point object defined for the trunk. |
|
Device Offline Polling Cycle Time |
Number |
Indicates how often all offline devices are polled. |
|
Device Online Polling Cycle Time |
Number |
Indicates how often all online devices are polled. |
|
Error Log |
One value from a set |
Shows the error log according to the last standard LonWorks network Query Status message. |
|
LON Integration DLL Date |
Date |
Displays the current date stamp on the LonIntegration.DLL. |
|
LON Integration DLL Size |
Number |
Displays the current size of the LonIntegration.DLL. |
|
LON Integration DLL Time |
Time |
Displays the current time stamp on the LonIntegration.DLL. |
|
Lost Messages |
Number |
Shows the number messages lost according to the last standard LonWorks network Query Status message. |
|
Missed Messages |
Number |
Shows the number messages missed according to the last standard LonWorks network Query Status message. |
|
Neuron Model |
One state from a set |
Shows the Neuron model according to the last standard LonWorks network Query Status message. |
|
Node State |
One state from a set |
Shows the state of the node according to the last standard LonWorks network Query Status message. |
|
Offline |
True or False |
Displays the offline or online status of connected hardware. The LonWorks network server updates this attribute value. |
|
Permanent Status Item Count |
Number |
Displays the number of items polled as a result of COV signups. |
|
Point Scan Time |
Number |
Displays the calculated number of seconds the server takes to read all defined points. |
|
Priority 1 Poll Item |
Number |
Displays the number of items in the Priority 1 list. |
|
Priority 2 Poll Item |
Number |
Displays the number of items in the Priority 2 list. |
|
Priority 3 Poll Item |
Number |
Displays the number of items in the Priority 3 list. |
|
Priority 1 Poll Time |
Number |
Indicates how often the items in the Priority 1 list are polled. |
| Priority 2 Poll Time |
Number |
Indicates how often the items in the Priority 2 list are polled. |
|
Priority 3 Poll Time |
Number |
Indicates how often the items in the Priority 3 list are polled. |
|
Receive Transaction Full |
Number |
Shows the number of times the transaction full message appeared in the last standard LonWorks network Query Status message. |
|
Reset Cause |
One cause from a set |
Shows the cause of the last reset according to the last standard LonWorks network Query Status message. |
|
Reset Date |
Date |
Contains the date stamp of the last local Neuron statistics reset command. |
|
Reset Time |
Time |
Contains the time stamp of the last local Neuron statistics reset command. |
|
Status Cache Hits |
Number |
Displays the number of READATTRIBUTE calls that occurred while the object was already being polled. |
|
Status Cache Misses |
Number |
Displays the number of READATTRIBUTE calls that occurred while the object was not being polled. |
|
Temporary Status Item Count |
Number |
Displays the number of items polled as a result of READATTRIBUTE calls. |
|
Transaction Timeouts |
Number |
Shows the timeouts that appeared in the last standard LonWorks network Query Status message. |
|
Transmit Errors |
Number |
Shows the number of transmit errors that appeared in the last standard LonWorks network Query Status message. |
|
Transmits Per Minute |
Number |
Displays the calculated number of transmissions per minute. |
|
Version Number |
Number |
Shows the version number according to the last standard LonWorks network Query Status message. |
|
XIF Present |
True or False |
Indicates whether the XIF is present. The XIF is a resource file required for the NAE to understand a particular device type. This attribute is not used in the SCT. |