Attribute Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
  • In the navigation tree, right click on the GIO object and select Commands then select an attribute for the GIO Attribute Command, and click the ellipsis button.

  • In a category view for the GIO (in the display frame), right-click on the attribute you want to command, and select Commands.

The attribute commands that appear are based on the data type of the attribute and whether Override Allowed and Adjust Allowed are True or False. See Table 1 for more information about these elements.

Table 1. Attribute Commands
Command Notes

Adjust ciz1559299015970.html#ciz1559299015970__fn_adjust_allow_must

Real values only (floating points)

Operator Override ciz1559299015970.html#ciz1559299015970__fn_override_allow_must

 

Release Operator Overrideciz1559299015970.html#ciz1559299015970__fn_override_allow_must

 

Change Units

All values but True/False

Change Name

 

Change Display Precision

Real values only (floating points)

State0...StateNciz1559299015970.html#ciz1559299015970__fn_adjust_allow_must

Two state or multistate values

Trueciz1559299015970.html#ciz1559299015970__fn_adjust_allow_must

True/False only

Falseciz1559299015970.html#ciz1559299015970__fn_adjust_allow_must

True/False only

1 Adjust Allowed must be True.
2 Override Allowed must be True.